EIP.PLLSTATE
Description
This parameter reads the state of the Phase-Locked Loop (PLL). The EIP.PLLSTATE can be queried in WorkBench terminal to report the current value and state of the PLL. Value 6 (Locked) indicates the AKD2G-SPI PLL is synchronized with the PLC.
|
Value |
Description |
|---|---|
|
0 |
Idle (not locked) |
|
1 |
Acquiring lock |
|
2 |
Searching for reference period |
|
3 |
Searching for phase lock |
|
4 |
Searching for frequency lock |
|
5 |
Fine adjust |
|
6 |
Locked |
|
7 |
Fault |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-10-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0 to 7 |
|
Default Value |
0 |
|
Data Type |
Integer |
| See Also | EIP.PLLMODE |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
EtherNet/IP drives: AKD2G-SPI
Industrial Ethernet
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3901 |
1 |
3901 (0xf3d) |
EIP.PLLSTATE |
Unsigned8 |
Read Only |
Yes |